This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2492: 请帮忙确认主要功能是否符合主要功能是processor还是controller的定义?不符合请提供主要功能

Part Number: TPS2492
Other Parts Discussed in Thread: TPS2493

Hi Team,

此型号datasheet 显示controller, 但是TI 提供的HS code为8542399000, 但是实际controller的HS code应该是属于854231.系列。

那么到底此型号的主要功能是符合processor还是controller的定义? 不符合的话才能符合HS code 8542399000, 那么请提供主要功能,谢谢

  • HI

        从你描述看是处理器的问题?但这里的电源管理芯片的论坛,所以不清楚你处理器的问题。

        同时没有看到关于TPS2492的描述? 

  • 这个系列在TI web上自动归为电源模块板块的。问题主要是这个datasheet写此类为controller,但是TI 自己提供的HS code不符合controller的定义, 那实际的主要功能应该是什么呢

    描述如下;

    The TPS2492 and TPS2493 are easy-to-use, positive high voltage, 14-pin Hotswap Controllers that safely drive an external N-channel FET to control load current. The programmable power foldback protection ensures that the external FET operates inside its safe operating area (SOA) during overload conditions by controlling of power dissipation. The programmable current limit and fault timer ensure the supply, external FET, and load are not harmed by overcurrent. Features include inrush current limiting, controlled load turn-on, interfacing to down-stream DC-to-DC converters, and power feed protection.

    The analog current monitor output provides a signal ready for sampling with an external A/D converter.

    Additional features include programmable overvoltage and undervoltage shutdown, power-good for coordinating loads with inrush, and a fault indicator to indicate an over-current shutdown.

  • HI

        从描述看问题和TPS2492/3没有什么关系,主要在于controller的定义,从你描述看就是处理器。