This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3409HV: 最小输出电压如何实现

Part Number: LM3409HV
Other Parts Discussed in Thread: LM3409

原理图如附件,输入48V,请问该驱动最低输入电压能到多少?
我测试发现,输出电压最低是7V,如果我想实现更低的输出电压,比如2V,我该如何处理?

  • HI

        为什么要确认最小输出电压,而不是按照你实际负载需求来做吗?

        这类芯片并没有给出最小duty,或者最小输出电压,如果你需要知道这个,你可以根据最小ton来确认。

  • Hi

      我使用LM3409驱动一个TEC,TEC可以看出是一个2Ω的电阻。电流调控范围是0~6A。(因为要实现一个大电流的调控范围,所以有个最低电压问题)

       依据下面描述中的参数配置,无法实现0~7V的输出,7V以上是可以正常输出的。

        假设我要实现4V~2A的输出,

       RC是使用72K+470pf,计算出toff是13091ns,ton是1522ns,频率68kHz(满足规格书的要求 toff最大300us ton最小115ns)
       电感使用15uh(原理图中是33uH,实际使用15uH,计算出电感纹波3491mA,满足电感最小纹波大于738mA

       采样电阻32.5mR(原理图中是55mR,实际使用32.5mR),LED电流可以实现5.89A的输出,我通过DAOUT1实现2A的电流调控。

     假设我要实现12V~6A的输出,

       RC是使用72K+470pf,计算出toff是3848ns,ton是1749ns,频率179kHz(满足规格书的要求 toff最大300us ton最小115ns)
       电感使用15uh(原理图中是33uH,实际使用15uH),计算出电感纹波3078mA,满足电感最小纹波大于738mA

       采样电阻32.5mR(原理图中是55mR,实际使用32.5mR),LED电流可以实现6.1A的输出,我通过DAOUT1实现6A的电流调控。

       但是上述2种假设只有2是可以正常输出的,假设一无法输出。

  • HI

       这个芯片最小4V输出应该是可以做到的,从描述看也满足datasheet规格要求,那出现的不良模式是什么?