Part Number: LM3409HV
Other Parts Discussed in Thread: LM3409
原理图如附件,输入48V,请问该驱动最低输入电压能到多少?
我测试发现,输出电压最低是7V,如果我想实现更低的输出电压,比如2V,我该如何处理?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
为什么要确认最小输出电压,而不是按照你实际负载需求来做吗?
这类芯片并没有给出最小duty,或者最小输出电压,如果你需要知道这个,你可以根据最小ton来确认。
Hi
我使用LM3409驱动一个TEC,TEC可以看出是一个2Ω的电阻。电流调控范围是0~6A。(因为要实现一个大电流的调控范围,所以有个最低电压问题)
依据下面描述中的参数配置,无法实现0~7V的输出,7V以上是可以正常输出的。
假设我要实现4V~2A的输出,
RC是使用72K+470pf,计算出toff是13091ns,ton是1522ns,频率68kHz(满足规格书的要求 toff最大300us ton最小115ns)
电感使用15uh(原理图中是33uH,实际使用15uH),计算出电感纹波3491mA,满足电感最小纹波大于738mA
采样电阻32.5mR(原理图中是55mR,实际使用32.5mR),LED电流可以实现5.89A的输出,我通过DAOUT1实现2A的电流调控。
假设我要实现12V~6A的输出,
RC是使用72K+470pf,计算出toff是3848ns,ton是1749ns,频率179kHz(满足规格书的要求 toff最大300us ton最小115ns)
电感使用15uh(原理图中是33uH,实际使用15uH),计算出电感纹波3078mA,满足电感最小纹波大于738mA
采样电阻32.5mR(原理图中是55mR,实际使用32.5mR),LED电流可以实现6.1A的输出,我通过DAOUT1实现6A的电流调控。
但是上述2种假设只有2是可以正常输出的,假设一无法输出。