Other Parts Discussed in Thread: BQ24630, LM3481
24V磷酸铁锂电池由几节组成?
用bq24630芯片是否只是给单节电池充电?其设置VREF=2.1V是否只是给单片电池的过放电压?
18V3A输入给24V10AH锂电池充电,电路可以有哪几部分组成?组成的每部分具体用什么芯片?其作用是什么?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
一般LiFePO4电池的标称电压是3.2V、终止充电电压是3.6V、终止放电压是2.0V,因此假若是7节,则通常可以标注为22.4V,这个24V标准比较特别,最好能和该电池供应商确认下!
Bq24630支持1-7节磷酸铁锂电池充电,因此单节只是其支持的一种应用。其VREF是3.3V啊?!这个是可以用来设定充电电流大小,适配器输入电流限流点和充电温度保护点的基准电源的。
18V3A输入要给24V10Ah充电,则首先需要将18V升压到至少26V/2A,这个可以用LM3481,然后再用Bq24630
您这个需求中有几点问题可以再探讨下:24V磷酸铁锂电池标称具体代表几节电池?18V 3A输入最大功率只有54W,而电池是240Wh的,即使效率做到100%,也至少需要5小时的充电时间,这点是怎么考虑的?!