This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3409 多片同时使用出现问题,大家帮帮忙。

Other Parts Discussed in Thread: LM3409, LM3431

同时使用了4片LM3409驱动LED颗粒,两路驱动电流设计为850mA, 另外两路为1.5A,现在发现以下几个奇怪的问题:

1、850mA 两路电流不一致,一路只有740mA, 另外一路有810mA, 电流会不断增长,不过增长缓慢,大概1秒涨2-5mA;

2、同时开4路时,电流都普遍跌落,1.5A 可能下降到只有900mA;

3、断掉三路电源(有一个磁珠连接电源),只开一路850mA, 电流会跌到只有640mA, 原来可达到约740mA.

因为板子比较小,布板的时候,LM3409芯片和其他功率器件(采样电阻,MOSFET,电感,二极管)不在同一面,是不是会有影响?

下图,一个是1.5A的驱动电路,一个是850mA 的驱动电路,分别各多加一路,就是4路了。

还有一张图是PCB图,红色线部分是电流方向。