各位专家老师好,我最近在用IR2110驱动半桥电路的时候出了点问题,改了好几天都不行,因此我现在想问一下TI有没有类似ir2110的驱动芯片。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI目前没有高压半桥驱动芯片,目前最高只有120V的产品,LM5100.
建议你可以采用驱动变压器驱动桥式的开关管。
Hi
如果要采用CT 变压器的驱动电路,你可以参考一下TI的UCC28950 全桥驱动电路.
见UCC28950 User guide: http://www.ti.com.cn/cn/lit/an/slua560c/slua560c.pdf 第二十六页全桥驱动电路。
我的问题是这样的:最近做全桥逆变,用了两个IR2110,每个相当于驱动一个半桥,我在网上找了好多IR2110的驱动电路,大致都差不多,我按照下面这个图焊了,但是2110的低端输出正常,高端不对,后来又在网上找了找,给VS和地之间加了4.7K的电阻,高端波形就出来了,很奇怪。。。因为好像别人在做全桥逆变的时候都没有加这个电阻,我在电子工程世界论坛上问,网友给我说的是自举电容小了。
我准备明天再去试试换个大点的电容看,总之这个驱动这一块是好了,但是现在又有新问题出现了,我是用matalab仿真后用149输出SPWM波的,然后在经过一个硬件死区电路输给IR2110再送到全桥的,现在硬件死区电路有问题,这个电路图我是网上找的
我焊出来后用示波器一看不对,不知道是我对这个图的理解对不对,U1我是用的7414,然后U2直接用导线接了,不知道这个硬件死区电路图中的U2到底是门电路还是?
还请各位专家老师帮我解答一下。
首先感谢您的回答,可能是我把问题没说清楚,我只是想用一个IR2110驱动两个mos管交替导通,然后加有一定的死区
我看了一下LM5100的datasheet,看起来好像可以,还有我想请问可以用TPS28225驱动两个mos管交替导通吗?
看了一下UCC28950的datasheet,感觉那个图好复杂,可能是我知道还太少吧,嘿嘿。
TPS28225也可以用作驱动半桥或同步Buck,这个芯片也是在低压场合用的,但是一个很重要的指标就是母线电压,你的应用中母线电压如果是34V,比较低完全可以考虑用TI的芯片替代如Richard介绍的LM5100等芯片,但是TPS28225因为电压偏低仍然不适合。
xuchao fan 说:首先感谢您的回答,可能是我把问题没说清楚,我只是想用一个IR2110驱动两个mos管交替导通,然后加有一定的死区
我看了一下LM5100的datasheet,看起来好像可以,还有我想请问可以用TPS28225驱动两个mos管交替导通吗?