This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问bq20z40-r1和bq29330配合能够测量两节锂电池(7.2v-8.4v)的电量吗

Other Parts Discussed in Thread: BQ29330, BQ20Z40-R1

请问bq20z40-r1和bq29330配合能够测量两节锂电池(7.2v-8.4v)的电量吗

  • 可以的,这两个器件组合起来可以管理2-4节锂电池串联的电池组,但需要注意芯片BQ29330需要单独接到每一个电芯上,如果你的电池被封装起来,芯片测量不到每一个单独电芯的正负极就不适用了。

  • 我想用bq20z65-r1,是不是就不用模拟前端芯片BQ29330了啊,这样外围的电路就简单了吧?还有bq20z65-r1提供的3.3v电压给单片机能够提供多大的电流呢?请快一点告诉我好吗,因为这个活蛮急的。。谢谢啊

  • 是的 ,BQ20z65-r1将BQ29330这个模拟前端集成在内部了,但外部的BQ249XX系列的二段保护芯片还是要加的。

    REG3.3最大输出电流极限值145mA,当温度和reg2.5输出电流比较高时,REg3.3V最大输出电流限制相应的减少,但最小也有25mA。