This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5176-Q1: 輸入32V、在高溫環境85℃下帶載問題

Part Number: LM5176-Q1
Other Parts Discussed in Thread: LM5176

LM5176-q1按照WEBENCH參考設計,直流電源輸入9~32V,輸出15V,最大電流3A,帶載測試電流約1A,發生下列問題:

(1)  輸入32V 、輸出15V,在常態環境(溫度25℃)、及 低溫環境(溫度-40℃)、運轉正常。

(2)  輸入32V、 輸出15V,在高溫環境(溫度85℃),幾秒後,停止運轉。經檢修確認是 Buck/Boost IC LM5176 元件的 pin 27 (HDRV1)與 pin 28 (SW1)短路造成 (連測3片板子都如此)。

請問出現這種問題,是什麼原因造成,要如何解?