Other Parts Discussed in Thread: TPS55340, LM2587, TPS40211, LM3481, TPS43060, TPS43061
你好技术支持:
现在有两节锂电池串联(6.6V~8.4V)输入,要求升压到12V/1.5A以上输出,要求内置MOS管,请问有什么好的芯片推荐?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
可以选择
TPS55340: http://www.ti.com.cn/product/cn/tps55340
LM2587/8: http://www.ti.com.cn/product/cn/lm2587
等等。
Hi
符合的芯片比较多, 可以用TI的wenench仿真软件来选型,见网站:http://www.ti.com.cn/tihome/cn/docs/homepage.tsp
也可以用电源管理芯片的“电源快速搜索”进行寻找: http://www.ti.com.cn/lsds/ti_zh/analog/powermanagement/power_portal.page
上述推荐的芯片开关电流都最小在5A, 可以实现低于6.6V的输入电压。
相关电路设计,你可以采用TI的wenench仿真软件.