BQ76940电池管理芯片,在充放电MOS管S极之间串联0.1uF电容的作用
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,两个串联电容的作用是防止高频高压
These will help bypass the high frequency high voltage pulse across either the FETs or the pack terminals. Two capacitors are used in series in case one is shorted. The voltage rating should be able to withstand the pack voltage in case one of the capacitors is shorted. You want the size large enough to carry a significant current but small enough not to interfere with battery operation and to have a good frequency response. 0.1 uF is a nominal, select a different value if desired.