Other Parts Discussed in Thread: LM3407
1.我使用lm3407做了一个PWM控制的恒流源,5V电源输入,可以正常使用。由于技术要求,原来5V单片机AVR产生PWM输出的,现在要改为3.3Vstm32产生PWM,不知道对LM3407是否有影响。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
高过2.4V视之为高,低于1.3V视之为低,故0/3.3V是符合这个PWM逻辑判定标准的。
高的典型值是1.9,为了保证绝对的高,是需要大于2.4的, 例如假设是2V, 有些芯片不一定会判定为高,所以要大过2.4V,才绝对被判定为高。
同样的道理也适用于下限1.3V的控制。
Hi
高过2.4V视之为高,低于1.3V视之为低,故0/3.3V是符合这个PWM逻辑判定标准的。
高的典型值是1.9,为了保证绝对的高,是需要大于2.4的, 例如假设是2V, 有些芯片不一定会判定为高,所以要大过2.4V,才绝对被判定为高。
同样的道理也适用于下限1.3V的控制。