大家好,
TI,有没有电源芯片输入10—12V,输出5V。输出电流3A ,电源限流3.5A以上。纹波小于100mV峰间波纹电压。LDO,DC_DC都行。给RF模块,用于北斗模块。
北斗模块发射电流≦3.0A。谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
这种方案TI有很多种,比如tps54340。你用webench工具可以选择合适的方案:
http://www.ti.com.cn/webench
RF应用建议选择传统电压或电流型电源
TPS62130: 17Vin, 3A Load, 高效低噪声DC/DC
http://www.ti.com/sitesearch/docs/universalsearch.tsp?searchTerm=tps62130&linkId=1
Regards
Yangwei Yu
021-6031 6339
LP DCDC, ALPS, PWR