Other Parts Discussed in Thread: TPS55010, UC3843
TI专家:
能帮忙推荐一款隔离电源芯片(模块也可以)吗,可以是5V转5 V定压的,要是12V转5V的话,输入要宽压范围的(最少也应在10V~15V),输出电流只要达到50mA就行了,只给一个隔离运放、一个ADC还有一个磁耦(用于通讯隔离的)供电,便宜一点的,谢谢~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
www.deyisupport.com/.../228.aspx,2011中文电源管理选型指南第51页对隔离型电源模块有详细描述,你可以选择DCV01或DCH01的相关型号,有5转5的。
你好,
推荐TPS55010,可以实现5V-5V隔离电源。
如果要求便宜,推荐使用UC3843反激电源,实现10-15V输入5V输出。
另外根据你的应用情况,应该要求低输出纹波。建议将隔离电源的输出设计为6V,再用LDO将6V降为5V,这样能降低纹波。LDO推荐TPS71550或者TPS71401。