This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

麻烦TI工程师推荐DC-DC芯片

Other Parts Discussed in Thread: TPS5430, TPS62133, TPS62130, TPS54320, LMZ22003, LMZ22005, TPS54290, TPS54292

现在板子用的是TPS5430,但由于此芯片
1、非同步,效率可以稍低;2、振荡频率低,导致电感和输出电容体积都比较大。

TI工程师可否推荐一款同步整流,振荡频率1MHz以上的DC-DC芯片,且市场上用的比较多的芯片。用的比较多的话,比较容易买到。

具体要求:输入电压,支持6V~16V,输出电流3A,输出电压能支持5V的输出。(最好能支持6.5V输入,5V输出)

非常感谢~~~~