This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3404: LM3404

Part Number: LM3404


DIMI口电压是多少伏,调光PWM是只要DIMI管脚输入后就好,有没有记忆功能,还是需要一直输出PWM

  • Hi

       DIM电压规格见datasheet第6页:DIM COMPARATOR, 大于2.2V为高,低于0.8V为低,所以一般都是I/O口3.3V/0V的PWM信号来控制。

       DIM为调光信号,高3.3V时LED有输出满亮度, 低(0V)LED 最低亮度即无LED电流.   PWM占空比即控制LED亮度(持续3.3V为100%亮度,持续0V为0%亮度)。

      所以DIM信号是持续的。