Part Number: LM2611
Other Parts Discussed in Thread: LM2733, , TINA-TI, TPS61170
LM2611 是否能设计成-150V输出,在SW引脚处加个高压MOS管,类似论坛种的LM2733输出高压电路;
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
LM2611是没法做的。
请问输入电压是多少? 输出电压-150V,最大满负载电流是多少?
输入5~9V,电流1mA就够了,用在APD偏置电压,希望电路简单一些,不要加变压器或电流镜像之类的电路(FB脚是负反馈),请问是否有合适的方案或芯片?
不能在SW引脚加一个高压的MOS同时改变反馈电阻,使-24变为-100V吗?
Hi
在上面的电路的基础上再增加一级chargepump即可,同时略微调整一下反馈,但是要注意下电流是否足够?
(一级输出是-24V, 二级输出是-48V,再增加一级chargepump就是-96V, 通过调整反馈使得原本的一级输出-25V, 那么第三级就是-100V)
如果是要-150V, 需要在增加一级(总共四级),那么第一级就是150V/8.
能否在LM2611 上增加chargepump,比如LM2611 先输出-30在加chargepump,LM2611 是NFB 电路更加简单
HI
应该是不可以的,原因是两者设计的架构不一样,你需要选择的是升压芯片(类似TPS61170)加chargepump来做。
一级输出是-24V, 二级输出是-48V,再增加一级chargepump就是-96V 这个三级输出是-72V吧,如果-24的话需要加48 72 96 120 144 168 5级的电荷泵,这个有点多,所以想提升第一级电压,比如输出-80,请问有合适的芯片吗?是所有的BOOST Converter都能按 类似TPS61170 的电路设计输出负压吗?
Hi
这样的chargepump加级是电压翻倍的,-24V, 翻倍就是-48V, 再翻倍就是-96V, 并非每次增加-24V.
是所有的BOOST Converter都能按 类似TPS61170 的电路设计输出负压吗?