This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA551 OPA552 TLV172

Other Parts Discussed in Thread: TLV172, OPA551, OPA552

你好,我在做一个LDO的仿真,通过仿真验证了不同运放对LDO输出电压纹波的影响。仿真设置输入电压为5.5V,并且有一个峰峰值为50mV,200kHz的三角波纹波。输出设为5V。

仿真结果如下,OPA551增益带宽3MHz:输出纹波3.36mV;OPA552增益带宽12MHz,输出纹波1.5mV;TLV172增益带宽10MHz,输出纹波18.49mV。下面是仿真模型和输出纹波仿真图。

我的理解中,增益带宽越高输出纹波越小,但是仿真结果却不是这样,是仿真模型有问题吗,还是有运放其他参数有影响。可以详细解释一下吗,谢谢。

  • 您好,您的这个问题和 e2echina.ti.com/.../opa551-opa551-opa552-tlv172 重复了,我看我同事也已经回复给您了。 有什么问题您可以直接在上面链接中跟进就好。所以这个相同的问题我暂时就先关闭了。