This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61500: 技术问题

Part Number: TPS61500

您好!

    我想问一个关于TPS61500的动作的问题。我参考Datasheet用TPS500设计了一款背光升压电路。电路动作正常,各个点的波形也正常。我们的产品需要做雷击测试(有相应的保护电路),

    在印加雷击电压之后。背光电路陷入了一种停止振动的状态,输出电压等于输入电压。此状态会一直保持,直到产品电源关闭后重新启动。或是将EN管脚强行接地1秒以上,

    否则TPS61500不会重新开始工作。

    印加雷击电压的瞬间在EN脚,VIN脚等处发生脉冲电压都能理解,瞬间的异常动作也能理解。但是,在雷击电压以后,我有测试各个管脚(VIN,EN,OVP,FB)均为正常电压(FB电压为0)。

    这样状态不是应该重新自动启动振动吗?Datasheet上关于此种现象没有任何描述。我也做过测试,将EN脚,VIN脚都强制设置为0V,在0V期间的确停止振动,但是一旦解除,就又开始振动。

    另外我还试过,在二极管后端输入超过OVP的电压,接触后也会恢复正常动作。

    我最想知道的是,是何种原因导致外接电压均正常(VIN,EN,OVP)但是持续无法振动的现象。这样才能针对此现象采取对策。

 谢谢!