This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54531: 输出电压降低

Part Number: TPS54531

之前有咨询过的问题一直没解决,现在又出现

一个板上用了3片TPS54531分别输出9V  5V  7V,7V这个故障概率较高,另外两个基本没故障过,原理图如下

7V的负载很小,最大只有100mA,最小50mA

故障板7V变为了4V,测得VSENSE端电压为0.45V  开关频率减半311KHz,BOOT管脚震荡比正常板严重些,BOOT管脚波形

正常板VSENSE端电压为0.8V  开关频率634KHz,BOOT管脚波形

我看手册介绍过流保护的地方,故障板的开关频率和VSENSE端电压,比较符合

7V这里也出现过直接把24V输入管脚烧糊的情况。

问题:

但是这个负载非常小,不应该这么大概率的过流吧,另外两片5V和9V的没出现过,这个故障是怎么导致的呢?

还有就是手册介绍低于160mA会进入脉冲跳跃的Eco-mode,但是从boot管脚波形来看,并没有,还是连续的开关频率,是为什么呢?