This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5156H: LM5166H出现输出电源跳变情况

Part Number: LM5156H
Other Parts Discussed in Thread: LM5156

您好,最近在使用LM5156H时出现了输出电源不稳情况,但不清楚问题出在什么地方。

我们的具体应用为:利用LM5156将5V升值12V,5V供电采用一般的USB供电,希望得到稳定的12V直流电源。但实测后的结果为输出在5V与12V之间来回跳变,示波器测得的波形如图:

进一步我们测量FB引脚后也存在电压跳变情况,具体波形如图:

我们当时推测是USB供电带负载能力不足导致,然后我们将此电路连接至数字电源,将电源输出设置为5V 1.5A则正常运行。但我们使用的电路经过先前验证可以通过USB供电并保证后续电路可以正常运行的,同一批次的PCB中仅此一块出现了此现象,我们想知道出现此现象的原因处在什么地方。

谢谢!