This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请帮忙推荐合适的LED恒流驱动方案,需要PWM脚控制恒流是脉冲输出

Other Parts Discussed in Thread: TPS92518

请帮忙推荐合适的LED恒流驱动方案,需要PWM脚控制恒流是脉冲输出,需求如下:

1)支持单路或双路输出;每路只串一颗LED灯珠;所以输出电压最大不超过5V, 典型值约2.5V ;
2)输出恒流最大2.5A ;
3) 输入电压24+/- 6 V; 所以是BUCK控制模式;
4) 需要使用PWM脚,或en脚控制恒流是脉冲输出;PWM频率2KHZ ;
5) 恒流输出响应PWM控制信号时间不超过5us ;

谢谢