TI E2E 英文论坛海量技术问答的中文版全新上线,可点击相关论坛查看,或在站内搜索 “参考译文” 获取。

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC25800-Q1: UCC25800

Part Number: UCC25800-Q1

Hi, 

I am developing a SIC based reference design and used the UCC25800 for gate drive bias power supply. I referred to your EVL board 基于UCC25800-Q1开环LLC驱动器的隔离电源方案设计 - 电源管理 - 技术文章 - E2ETm 设计支持 (ti.com) and used the same schematic and selected the same components value. but wen I power it on with 13.5V/15V input, it can't start. A very interesting phenomenon, when I put a digital multimeter on the both end Pin 4(OC/DT) and AGND with DC voltage stalls, it starts correctly and when I remove the probe, it still works normally. 

it seams that OCP occurs even with soft-start and I tried to add a 33nF capacitor between VREG and RT to increase the soft start timing, no any improvement.

Below is my schematic, could you please help check and if you have suggestions? Looking forward to your feedback with many thanks!

Kevin

  • Hi 

    The problem has been solved, the voltage on OC/DT is too critical and a little higher than 3.95V and it triggers the DT-out-of-range fault and the driver shuts down, I changed R106 form 12.4k to 11k, it works normally, thank you!