This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92692: 芯片PDRV引脚的作用

Part Number: TPS92692

目前我们在用这个芯片,PDRV(12脚)一直都空着,BOOST拓扑,输入电压13.5V,输出电压43V,输出电流400mA,当10脚不注入PWM的时候,负载没有问题不闪烁,当对10脚注入200Hz,10%的占空比的时候,负载出现明显闪烁。

我尝试了两种方案:

1.当我尝试把输入电压提高到20V或者更高的时候,空着DPV引脚,此时向10脚注入PWM,不再出现闪烁;

2.当我把PDRV引脚接上PMOS接入负载,13.5V下不再闪烁;

问题:

1.芯片PDRV引脚的作用,如果我不使用PWM调光是不是可以省略;

2.或者我在输入输出压差不大的情况下不使用PDRV引脚,是不是也可以进行PWM调光,只是效果差一些?