Other Parts Discussed in Thread: TPS61040, TPS61085, TPS61087, TPS61170
想用 TPS61040(400-mA )做一个5V/1A输入,13V/200mA输出的一个电源,只知道手册上说该器件在400mA时内部开关判断,但是能输出13V/200mA吗? 暂不考虑其它条件,只想确认器件本身是否可行
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
粗略计算输入平均电流为520mA,平均值已大于mosfet 400mA峰值限制,不建议用此器件
可考虑TPS61085
http://www.ti.com/lit/ds/symlink/tps61085.pdf
输出功率=13*0.2=2.6W,输入电压5V,则要求的输入平均电流约为0.52A.....因此不能正常工作,可以选择tps61087 或TPS61170