各位高手,我要给MSP430F448的3.7V、2000mAh锂电池( -40℃~+55℃)做一个充电器。请各位给个参考方案。谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位高手,我要给MSP430F448的3.7V、2000mAh锂电池( -40℃~+55℃)做一个充电器。请各位给个参考方案。谢谢
你好,请问能提供更多详细的信息吗?charger想用I2C控制还是standalone?需不需要DPM.这个项目应用在什么地方?另外你的充电器是指包含了适配器的吗?
如果没有特殊需求,从你的2000mAh电池 充电电流一般会大于1A,建议采用开关类型的,比如BQ24253。谢谢!
您好,我们以前做了几款手持式光纤物理链路检查仪,采用普通3节1.5V电池供电,现在要改为锂电池供电。以前的检查仪电路不想改动,将原有普通电池更换为锂电池,外部增加AC-220V和DC-28双输入的充电器,对锂电池供电。
DC28V输入可以看下BQ24610是否满足需求?AC-220部分可以考虑使用UCC28700,http://www.ti.com/product/ucc28700,页面右边有一个WEBENCH工具可以帮助更快地进行设计。
楼主 正如Sheldon的建议,架构上可以用一个flyback 的电路将ac220降低到接近28v ,然后做一个输入源二选一的电路(AC220V转的Dc电压优先供电),或者看是否有本身兼容两个输入源的充电器
推荐你参考一下这里,有很多方案:
http://www.deyisupport.com/question_answer/analog/battery_management/f/35/t/4945.aspx