This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tps70950 输出90mA就保护了对么???



70950的使能脚我用的是LM336 2.5 V 的稳压管,输入输出的电容都是焊的2.2uf/35V 的钽电容,输入电压为18.8v,我测70950输出电流为90mA左右就会保护出现一个35ms的下降沿脉冲然后在拉会正常,一会又变低周尔复始,设备不能正常工作为啥?

报警语音.PCB
  • Hi

       TPS70950对输出电容ESR的要求是0~0.2欧姆,才能稳定输出。

       所以首先确认一下你的2.2uF钽电容的ESR是否符合条件?按照datasheet要求,一般都是用X5R,X7R的低ESR陶瓷电容。(如果你手头没有陶瓷电容,可以用2个钽电容并联看看,layout(焊接)靠近芯片Vout脚,ESR满足要求)

       其次你的输入电压比较高,导致LDO功耗比较大,当输出电流在90mA以上(按照你现在的条件,输出在150mA之前一定会热保护的),环境温度30℃时,芯片温度已经在120℃左右了,虽然是158℃热保护,但是也建议确认一下(如果不是输出电容导致的不稳定).

  • Hi

       请问,是否有确认问题所在?