This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

找开关电源芯片

Other Parts Discussed in Thread: TPS54428, TPS54540, TPS54340, TPS62130, TLV62130, TLV62130A

应用环境:12V 2AH蓄电池供电,转3.3V电源供电,需要能工作一周,

需要找的芯片:DC电源芯片在运行时电流能尽量小,看了TPS54428/54228,运行电流在1mA比较大(不是shutdown时的),因为DC是一直开着的。

麻烦TI工程师帮忙推荐一款DCDC芯片,希望能满足条件,同时价格尽量低些。

谢谢!

  • 你好,

    TPS54428带有Eco-Mode功能,此功能能在轻载时实现自动跳周期来获得轻载高效。

    请问你在12V转3.3V时需要带几A负载,或者平均下来是几A,比如12V 2AH蓄电池的最大能量就是24WH,那么转3.3V 1A就是3.3W,可以工作的最长时间就是7.27H,如果加上转换器的损耗时间则更短。

    实际上DCDC转换器运行时,本身消耗的电流并不太大,应该所占影响的比例不重,最关键的还是你的负载是多大,理论上能不能达到一周。谢谢。

    Best Regards,

    Randy Wang

  • (1)正如楼上所说,要想进行选型除了需要知道12V~3.3V,输出电流也是一个关键因素,必须知道;

    (2)看了你的需求工作一周,应该是需要高效率,那么你需要的应该是开关型的器件;

    (3)开关电源的效率基本可以达到90%,如此你再根据你电池的容量可以计算出你的电池是否可以续航一周;

    (4)TI提供的芯片,例如之前所说的TPS54428等均带有ECO mode,轻载高效在市面具有很大的优势,推荐使用;

    (5)目前,开关型的器件主流又分为controler和converter,从你关心的效率上来看,这两者没有太大的区别,所以还得根据你的其他需求来选,例如价格、体积等;

    (6)所以,如果需要推荐选型希望您下次可以把需求说的更清楚一些。在这里,我推荐你上去这个链接,选择buck型、输入输出电压、电流等参数进行选型:http://www.ti.com.cn/lsds/ti_zh/analog/powermanagement/power_portal.page

  • 你看看tps54340/54360 tps54540/54560这几颗一百多uA的电流满不满足要求?

    另外,由于输入是12V的蓄电池,可能会有较大的浪涌电流,所以要选输入耐压高达40V的芯片。

  • 推荐TPS62130,采用DCS控制技术,轻载高效,最高耐压17V.

    http://www.ti.com/product/tps62130

     

    Regards

    Yangwei Yu

  • Hi

        或者选择TLV62130/TLV62130A, 与TPS62130差不多,但是芯片成本更低:   http://www.ti.com.cn/product/cn/tlv62130

        19uA超低的静态工作电流,100%占空比可以适应更低的输入电压,Power-Saving模式降低轻载损耗。