Other Parts Discussed in Thread: BQ24070, BQ24172
两个问题:
1 做手持设备,单节锂电池,使用BQ24070做电池充电管理芯片的时候,客户使用时候可能出现这种情况,取下电池,只接5V输入的AC适配器,这个时候Vout是否可以单独输出4.4V电源给系统供电? 另BQ24070手册中写到“4.4-V and 6-V Options for System Output Regulation Voltage”,是否表示BQ24070内部设计有电路可以将单电池升压到4.4V恒定输出,还是BQ24070最高输出到4.4V,当电池是3.8V的时候,BQ24070的输出也就最高到3.8V?
2 当使用BQ24172的时候,我做了个测试:只接1节锂电池,供电也是输入5V适配器,当移走电池的时候,是无法输出5V给系统供电的,而输入是6V以上的适配器,是可以移走电池,可以通过适配器单独供电的,是否表示BQ24172在单节锂电池供电的应用中,是必须接电池的,不能移走电池只接5V适配器单独给供电?
谢谢