This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65251长期工作后3.3V电压输出偏低到3.0V上下



TPS652513路输出分别为5.0V 3.3V 1.0V,3.3V输出负载为2.5A,长时间工作后3.3V变为2.9V~3.0V,两款机种因此造成异常

1、机种一:出现该现象后重新焊接了一下反馈电容恢复正常,后续再无法模拟到现象。

2、机种二:一样的状况也出现在同样的设计的另外的一款产品上,当设备放置一段时间后开启电压恢复正常,不知道哪个环节出现问题。

怀疑热的问题,机种一用热风枪吹也无法付现

TPS65251.pdf