Other Parts Discussed in Thread: LM3914, BQ34Z110
我需要监测一个12v 8ah的铅酸蓄电池电量,它能分段显示(10.8v-13.8v)电量,并不需要智能管理,但要低成本、最易用和最简易的外围电路,除了lm3914我还有什么其他的选择啊?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
推荐使用BQ34Z110。
非常感谢您的回复,但这个BQ34Z110 对于我来说不是太实用,且价格偏高。
另外想问下,关于lm3914的应用问题。
我现在正在设计一个基于lm3914的电量监测电路。但遍查资料都发现其4pin都是对地应用(即0v-xv应用),我想让其显示(10.8v-13.8v)之间每段0.2v电压显示这样的功能,是否能实现,外围电路应该如何设计(lm3914工作电压也是使用同一电源)。另外,4、5、6、7和8pin之间的关系如何确定,所谓这几个引脚又该如何正确理解。
另外请教下,lm3914是否可以监测超出其工作电压的电压值,如200v-240v,如果可以这样的电路如何设计。