This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
IC框图中的CHRG_OK 引脚是否一定要加上拉电阻?
您好,建议加上10kohm的上拉电阻。
您好,请教个问题,现在发现在12V 2A 的输入下给2cell 充电的情况下,电感发烫严重,这有可能是那里导致的,电感容量为1uH
在SW1 SW2所NC得电路作用是什么的
您好,电阻-电容(R-C)缓冲器来抑制振铃
您好,电感发热严重建议抓一下HIDRV2, LODRV2,SW2,SW1的波形。
您好,谢谢您对上述问题的解答,我拿示波器看了一下SW1的波形,,并不是整齐的方波
为调试方便,我在Q2的G极串联了一个10欧姆电阻,这个电阻是否与150pF 构成一个RC电路,造成 LODRV1的开关延迟呢
这个IC在进行降压充电时,Q1和Q2是不能同时导通是吗,类似于DCDC中的同步整流