Other Parts Discussed in Thread: UCC27201, TPS28225, UCC27528, UCC24610
有源钳位正激自驱动空载功耗太大,TI有没有IC驱动的方案?或者有没办法在轻载是关闭同步整流?
还有,参考设计PMP4844中的同步整流驱动有什么优势?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI有IC驱动方案的,例如ucc27201。PMP4844中的驱动应该是TPS28225 驱动同步整流器。推荐看看这篇文章(有中文版的):
Operation and Benefits of Active-Clamp Forward Power Converters:
http://www.ti.com.cn/cn/lit/an/snva591/snva591.pdf
附带参考设计电路图:
http://www.ti.com.cn/cn/lit/ug/snvu096/snvu096.pdf
希望对你有所帮助。
你可能误会了我的需求
ucc27201和TPS28225都是MOSFET驱动IC,但不是同步整流驱动IC。
你好,
1.同步信号还是选择传统的变压器次级的信号比较好;
2.驱动IC用UCC27528这种,但是驱动电流比较大,注意加串联电阻;
3.轻载关闭同步整流的建议:在输出端做一个电流检测电路,当电流很小时,关闭UCC27528的使能ENA/ENB。
jianfei chen 说:你是要求内部集成同步整流驱动的controller么?
类似IR1168,SP6002这些
[/quote]
UCC24610用在正激不太好吧,要两个呢