This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于BQ24650 应用中的问题,望及时回复

Other Parts Discussed in Thread: BQ24650, LM324

1:我使用IRL7833替换SI7288,静态功耗增加了20mA.请问我做大功率设计120W输入,18V/6.6A时如何选择MOS管,并且不增加静态功耗呢?另外功耗增加的原因是什么呢

2:在上述大功率设计时BQ24650发烫很严重,请问如何散热,是否增加一层PCB为其散热比较合理,会不会增加EMC辐射呢?

3:MOS管不管如何选择,因为DC-DC转换时都会有损耗,所以是不是都会发烫严重,需要另外增加散热片。BQ24650的DEMO跑4A温升都很高了,应该跑不了10A,发热会太严重。

4:在MPPT设置时,BQ24650 Datasheet中使用LM324来进行太阳能板的温度补偿,那是不是LM324需要贴在太阳能板上面呢?如果是这样从工艺角度来讲并不合适。我使用了MCU加DA的方式,在测试环境不变的情况下,通过DA对mppset引脚进行扰动,这样是可行的,但是有个问题点,就是当扰动之后扰动10MS之后),我通过MCU检测输出电流的值还是有些波动,导致我每次扰动时都无法精准的获取到功率最大值,只是大部分这个最大值我是获取得到的,少部分因为扰动后电流检测不准所以未能在最大值。请问有办法解决MPPT跟踪问题吗?总感觉没做到很理想。

irl7833pbf.pdf