This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS548A29: 恒流输出振荡问题

Part Number: TPS548A29

我是用TPS548A29制作了一个恒流源,输入12V,输出15A@1.8V, 采样INA181A作为电流采样反馈的FB脚,开关频率700kHz,电源输出平均电流是15A,但是大致有个1A的纹波,这个不是开关频率造成的,看起来是控制环路引起的,我分析是这样的设计仅能控制平均电流,由于TPS548A29占空比可以大于50%,因此在电流上升发生了次谐波振荡,有什么方式可以解决