Other Parts Discussed in Thread: TPS40210, LM2622
我用SwitcherPro 设计boost电路,输入最小6V,最大7.2V,输出12V 0.3A,显示效率最大87%
请问 实际使用中如何提高效率?
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好:
正确的器件选型对于提高效率也是很有帮助的。针对你的输入输出要求,如果想要更高效率的电路设计可以选用其
他芯片,比如: TPS40210、LM2622。
可以使用网页左边的WEBENCH软件对TPS40210电路进行优化设计。