This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR36520: 关于这颗料软起时间问题及DCDC启动过程问题

Part Number: LMR36520

电路图如上,DC48/DC12的去向和各去向的电容如上图

在线设计工具用的不好,这个型号里面的后缀都没有直接可用模型,就没有用在线工具设计,同时,在线工具给出的一般设计电容值很小,电感值也小,实际是电容便宜,通常给的大。这个电感的电流纹波系数给的是0.4,电感饱和电流0.6A.

电路都焊好了,不给负载,只焊接图示部分,可以输出期望值。

这个DCDC理论知识不是很强,现在想咨询几个问题:

1.请问下这个是怎么进行内部软起的?

2.buck的占空比近似等于输出比输入,这个启动过程是占空比近似从0增大到0.25吗?启动过程是个什么样子,猜不出来。

3.这个设计有哪些问题?TPS5430DDA这颗料发过帖子,累计500颗左右,电源坏的故障率3%了,等有空再发个帖子问问。