Other Parts Discussed in Thread: TPS62089A
TPS62993可以满足输入电压范围为5.2--5.4,输出5V吗?或有其它芯片推荐满足输入5.2--5.4V,输出5V?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TPS62993可以满足输入电压范围为5.2--5.4,输出5V吗?或有其它芯片推荐满足输入5.2--5.4V,输出5V?
HI
电流多少? 如果电流较小,可以的,因为芯片可以工作在100% duty. 但是电流大了,就不行,例如如果高边MOS Rdson是80mohm, 电流3A, 电压损耗就是0.24V, 如果5.2V输入, 最大就是5.96V输出,如果Rdson在更加大,输出电压更加低。
HI
几百mA,用TPS62993是可以的。
或者可以选TPS62089A之类,
也或者可以在降压芯片list中选择100%duty的芯片: www.ti.com.cn/.../products.html