This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC59116-Q1: 输出电流,芯片级联,灯珠阳极电压要求

Part Number: TLC59116-Q1
Other Parts Discussed in Thread: TLC59116

您好,电路方案是:单独控制128颗灯,每颗灯有效电流为15~100mA,灯珠VF=2.85V;

问题1:Rext要设置为187.5Ω吗?
问题2:需要用8个TLC59116级联,有什么注意事项吗?
问题3:128颗灯珠的阳级接到同一个电压上,这个电源电压需要什么范围?
问题4: 这块表达的内容不太明白,麻烦详细说明一下
问题5: 这块表达的意思是:最小的Iout只能是50mA吗?【我们希望电流在15mA~100mA】

以上 还请工程师详细解答下 非常感谢,祝您新年快乐