Other Parts Discussed in Thread: LM3253, TPS54260, TPS2553, TPS54340, TPS54620
给GSM/GPRS无线数据模块供电,输入5V,3.8V输出,峰值电流至少3A,请问该选用TI的哪款稳压芯片?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
射频模块的电源选型可以到这里:http://www.ti.com.cn/lsds/ti_zh/power-management/rf-dc-dc-converter-products.page#p451max=2.5;3
根据你说的电流要求3A,猜想你是想要LM3253:
Hi
GSM/GPRS供电要求低noise,低纹波等,在TI官网上暂时仅仅找到TPS54260的方案:GSM /GPRS Power Supply from TPS54260: http://www.ti.com.cn/cn/lit/an/slva412/slva412.pdf 虽然它是2.5A输出芯片,但是按照描述0.1 A to 3 A GSM Pulse, 看起来一样是可行的。
供电方面,虽然TPS54260可以达到60V供电,但是最低电压3.5V,也是符合你的要求的。
但是我觉得非常多的芯片都可以做到这个效果,例如: http://www.ti.com.cn/product/cn/tps62090 之类,同步降压效率还非常高,设计时可以将输出电容稍微放大一点。
看来你不是要找专业的射频模块电源,只是普通的DC电源的话那选择是很多的。例如你这里就是一个电压控制型的buck converter,内部集成了MOS或者二极管,这种片子TI很多的。帮你看了一下,7V以下的buck converter有304种,符合已经给出的条件的大概还有50种。个人建议只是要求电压和电流没有特殊要求的话没有必要纠结这个型号。选出来的电路跟这个是差不多的。
http://www.ti.com/paramsearch/docs/parametricsearch.tsp?family=analog&familyId=751&uiTemplateId=NODE_STRY_PGE_T&virtualTreeURL=D_ATTRIBUTE_3001163|EQ|Yes&filter=a1163|EQ|Yes#p634max=4;6.5&p634min=0.6;2&p32=1;1&p451max=3;15&p1129=Synchronous%20Buck
你好,输入输出压差只有1.2v时,用非同步芯片在空载时输出会不稳。参考http://www.ti.com/lit/an/slva547/slva547.pdf
推荐tps54620或者优化了的非同步芯片tps54340/360。
Hi
你电路图的中的芯片确认是TI的吗? 有没有marking, 按照条件搜索,10pin脚的芯片中没有找到。