Other Parts Discussed in Thread: OPA2211A, TPS7A30, TPS7A49, TPS7A33, TPS7A47
本人之前购买了TI的OPA2211A精密运算放大器,想利用它对双频激光器输出的激光进行拍频探测。OPA2211A的链接如下:
http://www.ti.com.cn/product/cn/opa2211a
当光强较强时,用OPA2211A所做的前置放大器输出信号很好。但当光强较弱时,例如光强为10uW时,此时光电二极管输出的电流约为4uA。因为OPA2211A的偏置电流和噪声都很低,感觉应当仍然能够探测到较好的拍频信号,但利用TEK示波器观测时却发现完全被噪声淹没了,只有FFT中能够看到有用信号的谱线。
之后我们寻找了一下原因,发现给OPA2211A供电的+-5V电源纹波峰峰值有30mV,而且FFT中的噪声谱线和电源噪声谱线基本一致。然后我们找了一个电源纹波峰峰值为10mV左右的+-5V电源,此时POA2211A输出信号信噪比果然上来了,能够看到基本的信号波形,但还是有很多噪声。因为我们没有更好的电源了,所以打算利用手里的设备重新做一个好一些的电源,所以想请教一下TI的各位专家和各位有经验的同志们。
我们手里现在有爱浦公司生产的功率为30W的AC-DC模块,链接里面最下面的那个:
http://www.aipu-elec.com/ch/ProductClass-96-1.html
它的输出电压为+-12V,输出电流为1.25A,纹波峰峰值为120mV。OPA2211A所需电压为+-5V,所以我们想通过电压转换将+-12V转换为+-5V,在转换的过程中最大限度的降低纹波。初步的想法是利用 TPS7A49 LDO 和 TPS7A30 LDO配合实现+-12V到+-5V电压的转换,希望能够把纹波降低到1mV以下。二者配合的链接如下:
http://www.ti.com.cn/analog/cn/docs/analogsplash.tsp?contentId=75583&DCMP=hpa_pwr_tps7a30&HQS=Other+OT+tps7a30-bbcn
但是和别人讨论时他们说12V到5V压降太大,不如利用二级甚至三级转换效果更好,例如利用7806先将12V转到6V,然后再转到5V。或是先将12V转到9V,然后转到6V,最后再得到5V。他们说每一级都能够一定程度上抑制噪声,三级下来就能够把噪声抑制的很小了。
本人不确定是利用一级转换效果好,还是利用二到三级转换效果好,毕竟电源纹波峰峰值有120mV,相比目标1mV相差100多倍,所以自己也没底。请教一个各位有经验的同志那种转换效果更好?如果方便的话,能否推荐一些转换电路或所用芯片,多谢各位!