This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

使用 LP8556-E00 背光电压突变

输入电压3.5V~5V

输出18V/60mA.

开机正常18V, 几分钟后电压直接跳跃到30V

寄存器的值全部默认值,更改A9h寄存器也没有用,请帮忙分析是什么问题

Iset电阻24K

Fset 0 接到地