This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

lm2594



您好,datasheet上写的建议是最大输入40V的时候,电感是100uH,我的电容是松下的HFQ系列,120uF/35V的电解电容,我的电感不是按照datasheet写的要求,我的是伍尔得的电感150uH的,而您的建议是不小于220uH的电感和输出电容不小于180uF,请问我该怎么选择?能不能麻烦您给我一些建议,包括您说的220uH的电感是什么系列,电解电容是什么牌子的什么系列?还有没有别的要求才能让我的2594工作?麻烦您推荐一下,谢谢!

我还有一个小问题,就是我的另一个线路板也想用您的2594HV,他的输入大概要到36V,负载可以到6A,这两个可以一种电路么?

谢谢您

  • 电解大些;对IC影响不大。电感略小‘IC也是可以工作的,只是发热及输出略有降低。这里的电感是线性电感;TDK等许多厂家都可以买到。建议不要被手边的元件束缚;否则会削足适履。2594HV是高压版本;没有本质区别,可以用。

  • 您能留个方便的联系方式么?谢谢,我的邮箱是mahongtu@qq.com,qq是331204500,我的元气件是按照别人的设计更改的,别人用这个方案实现了,可是我的不行,我还用了ss16,请问输入电容是必须的么?线性电感能达到150uH么?您能推荐下具体型号么