Other Parts Discussed in Thread: TMP275
为什么我的TMP275不管是配置成几位精度,读到的温度都是整数在变,就是一度一度的变化,小数部分不变
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
给我看看,我的程序,我的也是这个问题
#include<reg52.h>
#define uchar unsigned char
#define uint unsigned int
#define NOP()
uint b,d,a1;
uchar n,r,a,d1,d2;
sbit SDA=P0^0;
sbit SCL=P0^1;
sbit W=P2^3;
sbit D=P2^4;
sbit LED=P2^0;
void display(uchar r);
void write_add(uchar point,uint date);
uchar code dtable[]={0x3f,0x06,0x5b,0x4f,0x66,0x6d,0x7d,0x07,0x7f,0x6f,0x80,0x00};
uchar code wtable[]={0x7f,0xbf,0xdf,0xef,0xf7,0xfb,0xfd,0xfe};
uchar table[7];
void delay(uchar z)
{
uint x,y;
for(x=80;x>0;x--)
for(y=z;y>0;y--);
}
void init()
{
SDA=1;
NOP();
SCL=1;
NOP();
n=0;
a=0;
b=0;
}
void start()//开始信号
{
SDA=1;
NOP();
SCL=1;
NOP();
SDA=0;
NOP();
}
void stop()//停止信号
{
SDA=0;
NOP();
SCL=1;
NOP();
SDA=1;
NOP();
}
void respons()//应答信号
{
uchar i;
SCL=1;//时钟线为高电平等待应答信号SDA
NOP();
while((SDA==1)&&(i<250))i++;//等待应答信号SDA=0;
SCL=0;//时钟线为低电平,控制总线暂停
NOP();
}
void write_byte(uchar date)//写一个字节
{
uchar i,temp;
temp=date;
for(i=0;i<8;i++)
{
temp=temp<<1;//左移一位
SCL=0;//SCL=0允许SDA数据可以变化,等待CY送到SDA上
NOP();
SDA=CY;
NOP();
SCL=1;//SCL=1,保持数据SDA稳定
NOP();
}
SCL=0;
NOP();
SDA=1;//总线释放
NOP();
}
uchar read_byte()//读一个字节
{
uchar i,k;
SDA=1;//释放总线
NOP();
for(i=0;i<8;i++)
{
SCL=0;//SCL=0允许SDA数据变化,等待读取数据到SDA
NOP();
k=(k<<1)|SDA;
SCL=1;//SCL=1,保持稳定,等待数据读取到SDA上
NOP();
}
return k;
}
uint read_add(uchar address)
{
uint date;
uchar date1,date2;
start();
write_byte(0x90);//写器件地址
respons();
write_byte(address);//写取寄存器
respons();
start();
write_byte(0x91);//读器件单元地址
respons();
date1=read_byte();
respons();
date2=read_byte();
respons();
stop();
date=256*date1;
date=date+date2;
return date;
}
void main()
{
init();
while(1)
{
d=read_add(0x00);//读0x00寄存器
d1=d/256;
d2=d%256;
d1=d1&0x7f;
a=d1;
d2=d2>>4;
d2=d2&0x0f;
b=625*d2;
if(a/100==1)
table[7]=1; //百位超过100度显示“1”
else
table[7]=11; //百位没超过100度,百威数码管熄灭
table[6]=a%100/10; //十位
table[5]=a%10; //个位
table[4]=10;
table[3]=b/1000; //小数点后第一位
table[2]=b%1000/100; //小数点后第二位
table[1]=b%100/10; //小数点后第三位
table[0]=b%10; //小数点后第四位
for(r=0;r<8;r++)
{
P1=0;
D=1;
D=0;
P1=dtable[table[r]];
D=1;
D=0;
P1=wtable[r];
W=1;
W=0;
delay(1);
}
}
}