Part Number: BQ79718-Q1
我是纬湃汽车电子长春工厂孙玉策,用的是咱们家的BQ79718芯片,我有个问题想要请教?
Control 1 command 0x309:我发送0x04命令进入sleep模式,然后我紧接着发送Control 1 command 0x309:0x10是不是就能回到Active模式?
相当感谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,请参考数据手册Figure 9-59. Power State Diagram
您好,请参考下面内容:
To transition the battery monitor from SLEEP to ACTIVE mode, the host must send either a WAKE ping/tone or SLEEPtoACTIVE ping/tone to transition to ACTIVE mode. The host must send the ping/tone because it cannot communicate with the device in SLEEP mode.
The WAKE ping/tone wakes up and resets the device, so the host will need to reconfigure the device setting. A SLEEPtoACTIVE ping/tone only wakes up the device.
Finally, wait (~10ms shutdown to active transition + ~600us propagation of wake) x number_of_devices, before attempting any further communications.
For more information, please see Section 9.4.1.3.3 of the datasheet and Section 3 of the Software Design Reference.