我们目前根据BQ24640应用电路,设计一款超级电容充电电路,该电路由隔离的电源模块15V输出给超级电容充电、给我们的MCU电路供电。超级电容2.7V/10F,5个串联,根据VFB和ISET设置的充电电压12.6V,充电电流500mA。
现在测试样板发现,充电电流较小,从50mA缓慢增长到300mA后(增长过程约1分钟)完成充电后充电指示灯熄灭,充完电后电容电压也只有10.6V左右。
与设计的充电电流500MA,电压12.6V不一致。BQ24640对超级电容充放电是怎么控制的?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,我司正在测试BQ24130芯片,按照超级电容充电电路搭的P9/29, 其中,我设置的充电电流为600mA,最后输出电压为8.4V,以上电路参数我稍做调整,其中R6,R7,电阻分别为10K,R9=33m,R2=65K,R3=100k,R12=0,R11空贴,PIN_CMOD=0V,CELL脚浮空
按以上电路搭了后,用万用表测试VREF脚为3.9V,给电容充电的电流为3mA,超级电容的电压在缓慢上升,上升到0.5V时候停止,其上升速度为0.001V/s,TS脚电压为1.9V,超电在充电的过程中发光管常亮,充电结束后发光管闪烁。
希望给出回复,谢谢。
QQ:51444449