BQ25713RSNR开机有12.6V的凸起。目前没有电池,请问是否可以修改寄存器改为8.9V。
如果改为8.9V,后续加上3cell的电池是否会影响充电?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,We would have to do more debugging to find out why. Do you know what the voltage of CELL_BATPRESZ is when this happens the voltage bump happens?
您好,CELL_ BATPRESZ determines the charge voltage and cell count.
With a voltage of 3.68, the charger thinks a battery is connected.
If the customer keeps having issues, you might be able to drive CELL_BATPRESZ to 0 V to stop the charging behavior.
您好,请参考下面内容:
There are many ways to do this to pull CELL_BATPRESZ low.
You can use resistors to pull CELL_BATPRESZ low. You can use a micro controller to do it.
Keep in mind, CELL_BATPRESZ sets the battery charge voltage, the minimum system voltage, and the SYSOVP voltage.
I have a question. There is no battery installed, CELL_ Isn't BATPRESZ supposed to be low by default? You mean if there is no battery, CELL_ BATPRESZ needs to be grounded directly and not connected to VDDA, right? Because all the schematic diagrams on the Internet have batteries. Please send me the schematic diagram without battery for reference.