最近使用到了TPS3823-33DBVR芯片,可是发现芯片的tt(out)时间各个芯片不统一,有1.8s的 还有1.2s的,因为我的芯片开机到初始化完毕输出喂狗信号大约要1.5s;所以1.2s的就不能用;datasheet中的TYP是1.6s(范围:0.9-2.5s);这种芯片不统一情况属于正常的么?有没有ttout时间更长的芯片?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
如果你在时间上做不到0.9s, 或者需要选择其他的芯片,但是查看了TI其他类似功能的芯片,例如TPS3305-33 ,他的Ttout时间规格是1.1~2.3S,相对于0.9s要长。
或者采用TPS3813K33, UCC2946这类Ttout可编程的设计。