给4节串联锂电池充电,利用bq24610参照datasheet上的电路搭建板子,没有用到热敏电阻所以就把R9和R10换成了10K。上电后是完全没有工作状态,检查电路是没有问题的,
求大神指点。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如果有改变FB 电阻值将其配置为4节电池充电的架构,观察输出端是否有观察到电池检测波形?是否有把电池插入验证一下。
此外实际的电路图如果和参考电路一致(修改为4节串联),那么是否有元器件因为实际采购的原因没有用参考电路图中的值,特别是电感器件。
和参考电路不一致的替换器件也希望能够一起附上来,芯片引脚的电压最好能附上来,这样可以给予很多分析的信息。谢谢!
没量错引脚,是我输入错了。我已经将RAC和RSB换回了10mΩ,R17也换回了10Ω;电感还是6.8,CTTC也换成了0.0563,另外PMOS用的是IRF9540,NMOS用的是IRF540;BAT54用1N5822代替。充电指示灯亮,直流电源箱的输出被拉低到5.8V。难道是我用的电源箱的问题?这个电源箱最大输出电流才1A
你好,为两节3000mAh串联的锂电池充电,选择bq24005可以吗?