Other Parts Discussed in Thread: LMZ12002
我现在输入12V,用lmz12002提供5V电源,用lmr10520tigong3.3V电源。再3.3V不进行数电转模电的情况下5V有400mV的毛刺,3.3V的毛刺更大。再接一个电感转出来的模电是他们毛刺会更大,而且3.3V电压变成0.9V。下面附上我的电路图和输出波形,我的电路板的原器件封装和PCB布局是按照说明文档来的。请教是什么问题导致的。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我测试用的安捷伦200mhz的示波器,按照我们平常的方法,以前测试过模拟信号,还是挺好的。
是空载测试的吗?带载试一试吧,看看是多少V
然后我想把3.3V的电源转换成模拟信号,用的是L2(10uH)和c7(0.1uf),然后3.3V出来变成0.9V,这是为什么啊。