Other Parts Discussed in Thread: TPS2376-H, TPS23754, TPS23756
I have an design need high power supply POE design,
so I select TPS2376-H,it is 802.3at type1 (high current) PD CONTROLLER,and the power level is 25W.and then I should bypass these 48V AC power line to an output to another POE device,and this device is 802.3at type1 (normal current),and the power level is 13W。Now i
have some questions about this design:
1:there are two different power levels on the PD side,does the PSE side(POE Switcher side) can recognize the POE device?or get the wrong power level?
2:If the PSE side(POE Switcher side) can only supply 13W,and the PD side power level is 25W,but PD only consumed less than 13W,does the PSE side can supply the power normally?
Merry Christmas&Happy New Year